Resistance Resolution NHS3152

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Resistance Resolution NHS3152

Jump to solution
1,798 Views
nicolas_woedy
Contributor II

Hello everyone,

I have a question/problem regarding the resistance measurement of the NHS3152. 

The data sheet advertises a Resolution of 0,83 Ohm at R(min) with the I2D-Range 250uA. The potentiometer I am using is working near the 400Ohm R(min), but I am not even close to 0,83Ohm resolution, even with max I2D conversion time. The steps are more like a couple of hundred.

Does anyone have advise what is necessary to get 0,83Ohm resolution?

 

Thanks

Labels (1)
  • RF

0 Kudos
Reply
1 Solution
1,791 Views
nicolas_woedy
Contributor II

Found the issue, porblem is solved.

View solution in original post

1 Reply
1,792 Views
nicolas_woedy
Contributor II

Found the issue, porblem is solved.