Resistance Resolution NHS3152

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Resistance Resolution NHS3152

ソリューションへジャンプ
1,805件の閲覧回数
nicolas_woedy
Contributor II

Hello everyone,

I have a question/problem regarding the resistance measurement of the NHS3152. 

The data sheet advertises a Resolution of 0,83 Ohm at R(min) with the I2D-Range 250uA. The potentiometer I am using is working near the 400Ohm R(min), but I am not even close to 0,83Ohm resolution, even with max I2D conversion time. The steps are more like a couple of hundred.

Does anyone have advise what is necessary to get 0,83Ohm resolution?

 

Thanks

ラベル(1)
  • RF

0 件の賞賛
返信
1 解決策
1,798件の閲覧回数
nicolas_woedy
Contributor II

Found the issue, porblem is solved.

元の投稿で解決策を見る

1 返信
1,799件の閲覧回数
nicolas_woedy
Contributor II

Found the issue, porblem is solved.