Resistance Resolution NHS3152

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Resistance Resolution NHS3152

跳至解决方案
1,796 次查看
nicolas_woedy
Contributor II

Hello everyone,

I have a question/problem regarding the resistance measurement of the NHS3152. 

The data sheet advertises a Resolution of 0,83 Ohm at R(min) with the I2D-Range 250uA. The potentiometer I am using is working near the 400Ohm R(min), but I am not even close to 0,83Ohm resolution, even with max I2D conversion time. The steps are more like a couple of hundred.

Does anyone have advise what is necessary to get 0,83Ohm resolution?

 

Thanks

标签 (1)
  • RF

0 项奖励
回复
1 解答
1,789 次查看
nicolas_woedy
Contributor II

Found the issue, porblem is solved.

在原帖中查看解决方案

1 回复
1,790 次查看
nicolas_woedy
Contributor II

Found the issue, porblem is solved.