RTC connections

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTC connections

Jump to solution
5,662 Views
Rocky4
Contributor II

Hi,

I want to use RTC - PCF85263A for my application. I will be connecting a Crystal of 32.768K Hz across OSCI, OSCO pins. 

Here I'm stuck with whether I should just connect only the Crystal to OSCI, OSCO pins? or I should also connect 7pF load capacitances to OSCI, OSCO pins along with the Crystal?

Because in the PCF85263A datasheet, internal capacitance selection option (through the oscillator control register) is provided.

Thank you in advance.

0 Kudos
Reply
1 Solution
5,653 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

The Cload depends on your selection crystal requirement CL value, if it need 7pF which just meet the RTC integrated 7pF that you don't need any external CL component.

 

View solution in original post

0 Kudos
Reply
6 Replies
5,654 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

The Cload depends on your selection crystal requirement CL value, if it need 7pF which just meet the RTC integrated 7pF that you don't need any external CL component.

 

0 Kudos
Reply
5,334 Views
Rocky4
Contributor II

Hi guoweisun

 

Thank you for the reply.

 

I need another clarification here. If I want to change the crystal, which has a load capacitance of 12.5 pF, in this case do I need to JUST CHANGE THE oscillator control register bits to 10 / 11 as shown below image.

                                                                     OR

I need to change the oscillator control register bits along with adding a load capacitors of 12.5 pF externally?

 

Thank you in advance.

Tags (2)
0 Kudos
Reply
5,283 Views
guoweisun
NXP TechSupport
NXP TechSupport

Please direct configure the register as 10 or 11.

0 Kudos
Reply
5,279 Views
Rocky4
Contributor II

Hi Guo-Wei Sun,

 

Thank you so much for the reply.

Just wanted to reconfirm that, If I configur the register to 10/11, then "adding a load capacitors of 12.5 pF externally" is not required now? 

0 Kudos
Reply
5,272 Views
guoweisun
NXP TechSupport
NXP TechSupport

Yes,after configure 10/11 you don't need add capacitor.

 

0 Kudos
Reply
5,269 Views
Rocky4
Contributor II

Hi guoweisun,

 

Thank you for the reply.

 

 

0 Kudos
Reply