RTC connections

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RTC connections

跳至解决方案
1,950 次查看
Rocky4
Contributor II

Hi,

I want to use RTC - PCF85263A for my application. I will be connecting a Crystal of 32.768K Hz across OSCI, OSCO pins. 

Here I'm stuck with whether I should just connect only the Crystal to OSCI, OSCO pins? or I should also connect 7pF load capacitances to OSCI, OSCO pins along with the Crystal?

Because in the PCF85263A datasheet, internal capacitance selection option (through the oscillator control register) is provided.

Thank you in advance.

0 项奖励
回复
1 解答
1,941 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

The Cload depends on your selection crystal requirement CL value, if it need 7pF which just meet the RTC integrated 7pF that you don't need any external CL component.

 

在原帖中查看解决方案

0 项奖励
回复
6 回复数
1,942 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Hi 

The Cload depends on your selection crystal requirement CL value, if it need 7pF which just meet the RTC integrated 7pF that you don't need any external CL component.

 

0 项奖励
回复
1,622 次查看
Rocky4
Contributor II

Hi guoweisun

 

Thank you for the reply.

 

I need another clarification here. If I want to change the crystal, which has a load capacitance of 12.5 pF, in this case do I need to JUST CHANGE THE oscillator control register bits to 10 / 11 as shown below image.

                                                                     OR

I need to change the oscillator control register bits along with adding a load capacitors of 12.5 pF externally?

 

Thank you in advance.

标记 (2)
0 项奖励
回复
1,571 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Please direct configure the register as 10 or 11.

0 项奖励
回复
1,567 次查看
Rocky4
Contributor II

Hi Guo-Wei Sun,

 

Thank you so much for the reply.

Just wanted to reconfirm that, If I configur the register to 10/11, then "adding a load capacitors of 12.5 pF externally" is not required now? 

0 项奖励
回复
1,560 次查看
guoweisun
NXP TechSupport
NXP TechSupport

Yes,after configure 10/11 you don't need add capacitor.

 

0 项奖励
回复
1,557 次查看
Rocky4
Contributor II

Hi guoweisun,

 

Thank you for the reply.

 

 

0 项奖励
回复