Hi,
I want to use RTC - PCF85263A for my application. I will be connecting a Crystal of 32.768K Hz across OSCI, OSCO pins.
Here I'm stuck with whether I should just connect only the Crystal to OSCI, OSCO pins? or I should also connect 7pF load capacitances to OSCI, OSCO pins along with the Crystal?
Because in the PCF85263A datasheet, internal capacitance selection option (through the oscillator control register) is provided.
Thank you in advance.
已解决! 转到解答。
Hi guoweisun
Thank you for the reply.
I need another clarification here. If I want to change the crystal, which has a load capacitance of 12.5 pF, in this case do I need to JUST CHANGE THE oscillator control register bits to 10 / 11 as shown below image.
OR
I need to change the oscillator control register bits along with adding a load capacitors of 12.5 pF externally?
Thank you in advance.
Hi Guo-Wei Sun,
Thank you so much for the reply.
Just wanted to reconfirm that, If I configur the register to 10/11, then "adding a load capacitors of 12.5 pF externally" is not required now?