Question about capacitance for the NX3L4051

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about capacitance for the NX3L4051

ソリューションへジャンプ
1,423件の閲覧回数
Sylvain2
Contributor I

Hi,

I'm interested by the NX3L4051PW-Q100J analog switch.

In the datasheet, I see values for "input capacitance" and "on-state capacitance". Can someone tell me the difference ?

I want to connect a coil to the input of the analog switch and I need to know what value of capacitance will be seen by this coil

 

Thank you!

Sylvain

0 件の賞賛
返信
1 解決策
1,418件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sylvain,

Input capacitance (Ci) is the internal capacitance seen at Sn (Select) and E (Enable) inputs. 

ON-state capacitance (Cs(on)) is the internal capacitance seen at the analog switch terminal when the switch is closed or ON. So this is the capacitance you need to consider.

Capture.JPG

 

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,405件の閲覧回数
Sylvain2
Contributor I

Thank you!

0 件の賞賛
返信
1,419件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sylvain,

Input capacitance (Ci) is the internal capacitance seen at Sn (Select) and E (Enable) inputs. 

ON-state capacitance (Cs(on)) is the internal capacitance seen at the analog switch terminal when the switch is closed or ON. So this is the capacitance you need to consider.

Capture.JPG

 

Best regards,

Tomas

0 件の賞賛
返信