Question about capacitance for the NX3L4051

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about capacitance for the NX3L4051

Jump to solution
1,424 Views
Sylvain2
Contributor I

Hi,

I'm interested by the NX3L4051PW-Q100J analog switch.

In the datasheet, I see values for "input capacitance" and "on-state capacitance". Can someone tell me the difference ?

I want to connect a coil to the input of the analog switch and I need to know what value of capacitance will be seen by this coil

 

Thank you!

Sylvain

0 Kudos
Reply
1 Solution
1,419 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sylvain,

Input capacitance (Ci) is the internal capacitance seen at Sn (Select) and E (Enable) inputs. 

ON-state capacitance (Cs(on)) is the internal capacitance seen at the analog switch terminal when the switch is closed or ON. So this is the capacitance you need to consider.

Capture.JPG

 

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
2 Replies
1,406 Views
Sylvain2
Contributor I

Thank you!

0 Kudos
Reply
1,420 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sylvain,

Input capacitance (Ci) is the internal capacitance seen at Sn (Select) and E (Enable) inputs. 

ON-state capacitance (Cs(on)) is the internal capacitance seen at the analog switch terminal when the switch is closed or ON. So this is the capacitance you need to consider.

Capture.JPG

 

Best regards,

Tomas

0 Kudos
Reply