Question about capacitance for the NX3L4051

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about capacitance for the NX3L4051

跳至解决方案
1,420 次查看
Sylvain2
Contributor I

Hi,

I'm interested by the NX3L4051PW-Q100J analog switch.

In the datasheet, I see values for "input capacitance" and "on-state capacitance". Can someone tell me the difference ?

I want to connect a coil to the input of the analog switch and I need to know what value of capacitance will be seen by this coil

 

Thank you!

Sylvain

0 项奖励
回复
1 解答
1,415 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sylvain,

Input capacitance (Ci) is the internal capacitance seen at Sn (Select) and E (Enable) inputs. 

ON-state capacitance (Cs(on)) is the internal capacitance seen at the analog switch terminal when the switch is closed or ON. So this is the capacitance you need to consider.

Capture.JPG

 

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,402 次查看
Sylvain2
Contributor I

Thank you!

0 项奖励
回复
1,416 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sylvain,

Input capacitance (Ci) is the internal capacitance seen at Sn (Select) and E (Enable) inputs. 

ON-state capacitance (Cs(on)) is the internal capacitance seen at the analog switch terminal when the switch is closed or ON. So this is the capacitance you need to consider.

Capture.JPG

 

Best regards,

Tomas

0 项奖励
回复