QI-Wireless power receiver MWPR1516

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QI-Wireless power receiver MWPR1516

Jump to solution
1,569 Views
Prabhath
Contributor I

In my custom wireless power receiver board using MWPR1516. I have a problem: after connecting the battery and attempting to charge it wirelessly for a few seconds, the power abruptly shuts off. Then I looked at the transmitter fault, which stated "Abrupt End of Power Transfer(EPT) initiated by the receiver." Does anyone have any ideas?

 

Thank you in advance.

0 Kudos
Reply
1 Solution
1,442 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the software issue please submit ticket here:

Home (nxp.com)

View solution in original post

0 Kudos
Reply
7 Replies
1,367 Views
Prabhath
Contributor I

I just add a series resistor with the battery then the power reception from the coil takes place. Then I reduce the value of the resistor up to a minimum of 0.4 Ohms(Only the lowest value in hand) and the power transfer still takes place. The measured voltage across the series 0.4 Ohm resistor was 1.48V. 

Additionally what changes I will need in the MWPR1516 demo application for achieving the 15W wireless charging? because I am suspecting the issue is related to the OCP or over-temperature.

0 Kudos
Reply
1,504 Views
guoweisun
NXP TechSupport
NXP TechSupport

You can refer to user guide for better understand and use it:

WPR1500BUCKMPUG.fm (nxp.com)

0 Kudos
Reply
1,454 Views
Prabhath
Contributor I

"Is there any issue with using the CodeWarrior free trial and the MWPR1516 software package provided by NXP? Because now I'm using this combination.

0 Kudos
Reply
1,443 Views
guoweisun
NXP TechSupport
NXP TechSupport

For the software issue please submit ticket here:

Home (nxp.com)

0 Kudos
Reply
1,533 Views
guoweisun
NXP TechSupport
NXP TechSupport

Do you change any transmitter board to try?

 

0 Kudos
Reply
1,421 Views
Prabhath
Contributor I

Is there any specification for coil 

0 Kudos
Reply
1,529 Views
Prabhath
Contributor I

Yes, I tried 3 different transmitters.

0 Kudos
Reply