PCF2131 is sending Acknowledgment

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCF2131 is sending Acknowledgment

跳至解决方案
2,311 次查看
PK_1114
Contributor II

Hai,

I am Working with the PCF2131is interfaced with the LPC54608 FC-7,

while Configuring the RTC it is going to slave not ACK state in I2C Bus Communication

PK_1114_0-1675335061456.png

 

 

Thank You,

B Pavan Kumar

0 项奖励
回复
1 解答
2,304 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

First of all, please double check that the IFS pin is connected to VDD:

Capture.JPG 

Then please make sure that the 7-bit slave address (1010011) is placed in the upper 7 bits of the byte and the write/read bit is in the LSB. This means 0xA6 for a write and 0xA7 for a read. Best is to check it using a logic analyzer or an oscilloscope.

Best regards,

Tomas

在原帖中查看解决方案

1 回复
2,305 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

First of all, please double check that the IFS pin is connected to VDD:

Capture.JPG 

Then please make sure that the 7-bit slave address (1010011) is placed in the upper 7 bits of the byte and the write/read bit is in the LSB. This means 0xA6 for a write and 0xA7 for a read. Best is to check it using a logic analyzer or an oscilloscope.

Best regards,

Tomas