PCF2131 is sending Acknowledgment

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCF2131 is sending Acknowledgment

ソリューションへジャンプ
2,270件の閲覧回数
PK_1114
Contributor II

Hai,

I am Working with the PCF2131is interfaced with the LPC54608 FC-7,

while Configuring the RTC it is going to slave not ACK state in I2C Bus Communication

PK_1114_0-1675335061456.png

 

 

Thank You,

B Pavan Kumar

0 件の賞賛
返信
1 解決策
2,263件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

First of all, please double check that the IFS pin is connected to VDD:

Capture.JPG 

Then please make sure that the 7-bit slave address (1010011) is placed in the upper 7 bits of the byte and the write/read bit is in the LSB. This means 0xA6 for a write and 0xA7 for a read. Best is to check it using a logic analyzer or an oscilloscope.

Best regards,

Tomas

元の投稿で解決策を見る

1 返信
2,264件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi,

First of all, please double check that the IFS pin is connected to VDD:

Capture.JPG 

Then please make sure that the 7-bit slave address (1010011) is placed in the upper 7 bits of the byte and the write/read bit is in the LSB. This means 0xA6 for a write and 0xA7 for a read. Best is to check it using a logic analyzer or an oscilloscope.

Best regards,

Tomas