PCAL6524 QFN Exposed Pad Connection

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

PCAL6524 QFN Exposed Pad Connection

跳至解决方案
2,591 次查看
mmWaver
Contributor I

Can someone please confirm if PCAL6524 QFN32 package's center exposed pad can/should be connected to ground?

Thanks!

标记 (2)
0 项奖励
回复
1 解答
2,577 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Paul,

The exposed pad underneath the PCAL6524HE (HUQFN32) is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

The exposed pad outline and the recommended footprint can be found at:

https://www.nxp.com/docs/en/package-information/SOT1426-1.pdf

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,562 次查看
mmWaver
Contributor I

Thank you Tomas for your reply!

0 项奖励
回复
2,578 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Paul,

The exposed pad underneath the PCAL6524HE (HUQFN32) is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

The exposed pad outline and the recommended footprint can be found at:

https://www.nxp.com/docs/en/package-information/SOT1426-1.pdf

Best regards,

Tomas

0 项奖励
回复