PCA9570 I2C Write/Read question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCA9570 I2C Write/Read question

1,003件の閲覧回数
Jay_Zhu
Contributor I

Hi Team

    I am confused about PCA9570 I2C write read, about the data1.

Jay_Zhu_0-1614929452419.png

As the Figure shown, Host need address PCA9570 firstly, and then send data1,data2.

So that's a question here, what the data1 make sense?

Is data1 Pin Mask?


I tried to enable P0 and I send 0x48 + 0xff + 0x01. P0 is enabled. 

But 0x48 + 0x01. Can not enable.

And 0x48 + 0x01 + 0x01. enabled also. And I see P0 has a shake , P1 too.

So I don't know what data1 need to be?

Jay_Zhu_1-1614929856688.png

 

Then the read reg, I will send 0x49 + data1?

data1 is port pin? like 0x01 means P0?

And what the data from PCA9570 means? All of pins' status? or just the data1 reponse pin I sent .

 

  

0 件の賞賛
返信
0 返答(返信)