PCAL6524 QFN Exposed Pad Connection

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PCAL6524 QFN Exposed Pad Connection

ソリューションへジャンプ
2,595件の閲覧回数
mmWaver
Contributor I

Can someone please confirm if PCAL6524 QFN32 package's center exposed pad can/should be connected to ground?

Thanks!

タグ(2)
0 件の賞賛
返信
1 解決策
2,581件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Paul,

The exposed pad underneath the PCAL6524HE (HUQFN32) is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

The exposed pad outline and the recommended footprint can be found at:

https://www.nxp.com/docs/en/package-information/SOT1426-1.pdf

Best regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,566件の閲覧回数
mmWaver
Contributor I

Thank you Tomas for your reply!

0 件の賞賛
返信
2,582件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Paul,

The exposed pad underneath the PCAL6524HE (HUQFN32) is not internally connected to any pin. It can be left floating, but for better thermal performance it is recommended to connect it to the GND.

The exposed pad outline and the recommended footprint can be found at:

https://www.nxp.com/docs/en/package-information/SOT1426-1.pdf

Best regards,

Tomas

0 件の賞賛
返信