Matching network for MMG20241H

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Matching network for MMG20241H

2,069 Views
stefanomoscato
Contributor I

Dear all, I will embed the MMG20241H wideband driver in an RF high power board for LTE communications. I have issues to reproduce with the circuit simulator the EVB matching network for 1700-2100 MHz band.

I used the S2P parameter, the transmission lines are well dimensioned (as datasheet reports) and also the substrate set is the same of the EVB.

Do you have any suggestions?

Thanks in advance for your priceless time!

Stefano

Labels (1)
  • RF

Tags (2)
0 Kudos
Reply
1 Reply

1,966 Views
andrei_skok
NXP Employee
NXP Employee

Please create a Service request for this issue.

How I could create a Service Request?

0 Kudos
Reply