MPC563/4 QADC Continuous Scan vs Single Scan

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC563/4 QADC Continuous Scan vs Single Scan

740件の閲覧回数
chrisjablonski
Contributor I

Hi,

I have a simple experiment set up to accept an analog input and route directly to a DAC output. Using a signal analyzer I am then measuring the frequency response. The gathering of the ADC result and assignment to DAC output are performed within a 4kHz interrupt. I get significant phase response differences between these two scenarios:

1) ADC is in continuous scan mode. Upon entering the ISR, the result is read and assigned to the DAC output. With this I get approx. 180 degrees of lag at 2.4kHz.

2) ADC is in single scan mode. Upon entering the ISR, the scan is triggered by writing to the SSE bit. I then wait until I see the completion flag CF, then assign to the DAC output. With this I get approx. 180 degrees of lag at 1.2kHz.

Can anyone help me understand why this would be? Is there anything HW related that would cause this? Is there a trick to initialization? I can't see anything in the documentation that would suggest an extra interrupt cycle delay.

Any/all suggestions are appreciated,

Thank you!

0 件の賞賛
返信
0 返答(返信)