MPC563/4 QADC Continuous Scan vs Single Scan

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC563/4 QADC Continuous Scan vs Single Scan

752 Views
chrisjablonski
Contributor I

Hi,

I have a simple experiment set up to accept an analog input and route directly to a DAC output. Using a signal analyzer I am then measuring the frequency response. The gathering of the ADC result and assignment to DAC output are performed within a 4kHz interrupt. I get significant phase response differences between these two scenarios:

1) ADC is in continuous scan mode. Upon entering the ISR, the result is read and assigned to the DAC output. With this I get approx. 180 degrees of lag at 2.4kHz.

2) ADC is in single scan mode. Upon entering the ISR, the scan is triggered by writing to the SSE bit. I then wait until I see the completion flag CF, then assign to the DAC output. With this I get approx. 180 degrees of lag at 1.2kHz.

Can anyone help me understand why this would be? Is there anything HW related that would cause this? Is there a trick to initialization? I can't see anything in the documentation that would suggest an extra interrupt cycle delay.

Any/all suggestions are appreciated,

Thank you!

0 Kudos
Reply
0 Replies