MPC5567: instruction execution cycles

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5567: instruction execution cycles

Jump to solution
2,727 Views
Afu
Contributor I
Hi,

I am looking for the execution time of the assembler/machine instructions. The document EREFRM.pdf (Reference Manual for BookE; chapt. 6: instruction set) doesn't list the clock cycles for each command. Where are they listed instead?

I am especially interested in the execution time of the "stmw" instruction.

Thanks in advance,
regards,
Afu.
0 Kudos
Reply
1 Solution
1,486 Views
dayve
NXP Employee
NXP Employee
Hello Afu,

The execution time for the instution set supported by the MPC5567 can be found within the e200Z6 reference manual. The timings are provided in the core reference manual rather than the BookE reference manual as different cores will execute instructions in a different number of cycles.

The e200Z6 reference manual can be found in the documentation section on the MPC5567 web page.

Regards,
David

View solution in original post

0 Kudos
Reply
1 Reply
1,487 Views
dayve
NXP Employee
NXP Employee
Hello Afu,

The execution time for the instution set supported by the MPC5567 can be found within the e200Z6 reference manual. The timings are provided in the core reference manual rather than the BookE reference manual as different cores will execute instructions in a different number of cycles.

The e200Z6 reference manual can be found in the documentation section on the MPC5567 web page.

Regards,
David
0 Kudos
Reply