MPC5567: instruction execution cycles

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5567: instruction execution cycles

跳至解决方案
2,725 次查看
Afu
Contributor I
Hi,

I am looking for the execution time of the assembler/machine instructions. The document EREFRM.pdf (Reference Manual for BookE; chapt. 6: instruction set) doesn't list the clock cycles for each command. Where are they listed instead?

I am especially interested in the execution time of the "stmw" instruction.

Thanks in advance,
regards,
Afu.
0 项奖励
回复
1 解答
1,484 次查看
dayve
NXP Employee
NXP Employee
Hello Afu,

The execution time for the instution set supported by the MPC5567 can be found within the e200Z6 reference manual. The timings are provided in the core reference manual rather than the BookE reference manual as different cores will execute instructions in a different number of cycles.

The e200Z6 reference manual can be found in the documentation section on the MPC5567 web page.

Regards,
David

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,485 次查看
dayve
NXP Employee
NXP Employee
Hello Afu,

The execution time for the instution set supported by the MPC5567 can be found within the e200Z6 reference manual. The timings are provided in the core reference manual rather than the BookE reference manual as different cores will execute instructions in a different number of cycles.

The e200Z6 reference manual can be found in the documentation section on the MPC5567 web page.

Regards,
David
0 项奖励
回复