MPC5567: instruction execution cycles

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5567: instruction execution cycles

ソリューションへジャンプ
3,641件の閲覧回数
Afu
Contributor I
Hi,

I am looking for the execution time of the assembler/machine instructions. The document EREFRM.pdf (Reference Manual for BookE; chapt. 6: instruction set) doesn't list the clock cycles for each command. Where are they listed instead?

I am especially interested in the execution time of the "stmw" instruction.

Thanks in advance,
regards,
Afu.
0 件の賞賛
返信
1 解決策
2,400件の閲覧回数
dayve
NXP Employee
NXP Employee
Hello Afu,

The execution time for the instution set supported by the MPC5567 can be found within the e200Z6 reference manual. The timings are provided in the core reference manual rather than the BookE reference manual as different cores will execute instructions in a different number of cycles.

The e200Z6 reference manual can be found in the documentation section on the MPC5567 web page.

Regards,
David

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,401件の閲覧回数
dayve
NXP Employee
NXP Employee
Hello Afu,

The execution time for the instution set supported by the MPC5567 can be found within the e200Z6 reference manual. The timings are provided in the core reference manual rather than the BookE reference manual as different cores will execute instructions in a different number of cycles.

The e200Z6 reference manual can be found in the documentation section on the MPC5567 web page.

Regards,
David
0 件の賞賛
返信