MAC7116

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,345件の閲覧回数
sudha
Contributor I
I am using MAC7116 with the external flash memory in a custom board.
The same is accessed with External Interface Module of MAC7116.
In basic , the MAC7116 micro shall be operated in either single chip mode / Expanded Mode.
I am using BDI2000 programmer.
I require the memory mapping while EIM is enabled and the procedure to configure the EIM.
Also how to decide the base address if EIM is used to access the external flash memory thru JTAG.
 
0 件の賞賛
返信
1 解決策
2,438件の閲覧回数
dayve
NXP Employee
NXP Employee
Hey!

Please take a look at AN2934 Using the MAC7100 EIM (External Interface Module). It will tell you how to configure the EIM as well as other information on using the EIM.

Once the external memory has been maped to an address you will be able to access it like any other memory address on the device. So you will be able to access it over JTAG.

Regards,
Dayve

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,439件の閲覧回数
dayve
NXP Employee
NXP Employee
Hey!

Please take a look at AN2934 Using the MAC7100 EIM (External Interface Module). It will tell you how to configure the EIM as well as other information on using the EIM.

Once the external memory has been maped to an address you will be able to access it like any other memory address on the device. So you will be able to access it over JTAG.

Regards,
Dayve
0 件の賞賛
返信