Hello,
I'm not sure where I can post this question.
I'm trying to use 2 audio codecs (same ones with same i2c slave addresses) with an PCA9543A, and I don't really know how to do it. So the alsa drivers will switch automatically between the 2 codecs, so they will be seen as 2 different audio cards.
In the init board, I think I have to :
- register the pca954x driver
- register the i2c-mux driver
- relate the pca954x to the i2c-mux and get the 2 created i2c sub-adapters
- and finaly instatiate 2 codec drivers with the i2c adapters
Example:
// Init board code
struct i2c_board_info i2c_info_pca954x[] = {
{
I2C_BOARD_INFO("pca954x", 0x70),
},
};
i2c_register_board_info(1, i2c_info_pca954x, ARRAY_SIZE(i2c_info_pca954x));
// How to register the i2c-mux driver?
// How to register the 2 codec drivers?
struct i2c_board_info i2c_info_codec[] = {
{
I2C_BOARD_INFO("tlv320aic3x", 0x18),
},
};
i2c_register_board_info(SUB_ADAPTER_1, i2c_info_codec, ARRAY_SIZE(i2c_info_codec));
i2c_register_board_info(NEW_ADAPTER_2, i2c_info_codec, ARRAY_SIZE(i2c_info_codec));
// Audio SOC code, declaration of the codecs
static struct snd_soc_dai_link davinci_codec1_dai = {
.name = "TLV320AIC3X",
.stream_name = "AIC3X",
.cpu_dai_name = "davinci-mcbsp",
.codec_dai_name = "tlv320aic3x-hifi",
.init = aic3x_init,
.codec_name = "tlv320aic3x-codec.SUB_ADAPTER_1-0018",
.ops = &ops,
.platform_name = "davinci-pcm-audio",
};
static struct snd_soc_dai_link davinci_codec2_dai = {
.name = "TLV320AIC3X",
.stream_name = "AIC3X",
.cpu_dai_name = "davinci-mcbsp",
.codec_dai_name = "tlv320aic3x-hifi",
.init = aic3x_init,
.codec_name = "tlv320aic3x-codec.SUB_ADAPTER_2-0018",
.ops = &ops,
.platform_name = "davinci-pcm-audio",
};
For now, when I register the pca954x driver, the pca954x_probe function is not even called, even if have the "i2c-core: driver [pca954x] registered" log.
Thank you in advance for your help.