Hi Experts,
I built a Debian Linux SDK24.06 image and deployed it to i.mx8 board.
The Debian Desktop boots successfully. But I find that many packages like imx-gpu-viv, cogl, libdrm, etc, are installed to rootfs by Makefile rather than the Debian package. The file libEGL.so.1.5.0 is installed to /usr/lib, meantime the libEGL.so.1.1.0 in /usr/lib/aarch64-linux-gnu/ installed by Debian package libegl1 is still there. These kinds of files are not under the control of Debian Package Management.
Is there a schedule that Fexlbuild creates a Deb Repository that contains NXP's deb packages?