Flexbuild: Debian Linux SDK24.06

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flexbuild: Debian Linux SDK24.06

Jump to solution
1,284 Views
quanyang_wang
Contributor II


Hi Experts,

I built a Debian Linux SDK24.06  image and deployed it to i.mx8 board.

The Debian Desktop boots successfully. But I find that many packages like imx-gpu-viv, cogl, libdrm, etc, are installed to rootfs by Makefile rather than the Debian package.  The file libEGL.so.1.5.0 is installed to /usr/lib, meantime the libEGL.so.1.1.0 in /usr/lib/aarch64-linux-gnu/ installed by Debian package libegl1 is still there.  These kinds of files are not under the control of Debian Package Management.

Is there a schedule that Fexlbuild creates a Deb Repository that contains NXP's deb packages?

Tags (1)
0 Kudos
Reply
1 Solution
1,253 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

There is no such plan.

Best Regards
Zhiming

View solution in original post

0 Kudos
Reply
2 Replies
1,254 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi

There is no such plan.

Best Regards
Zhiming

0 Kudos
Reply
1,249 Views
quanyang_wang
Contributor II
Got it. Thank you for replying.
0 Kudos
Reply