kernel panic with booting eMMC on imx8navq

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

kernel panic with booting eMMC on imx8navq

2,328件の閲覧回数
mmt45
Contributor I

Hello, I was following this guide to setup cognipilot on NavQPlus (imx8navq) https://airy.cognipilot.org/cranium/compute/navqplus/setup/#log-in-for-the-first-time ). After flashing the ubuntu image, I change the switches of Navq into eMMC mode (switch 1 off, switch 2 on), and when I screen into the UART connection from the terminal, I get a kernel panic error. It shows in the lines above that is related to ext4-fs. How can i solve the problem?

0 件の賞賛
返信
2 返答(返信)

2,279件の閲覧回数
Manuel_Salas
NXP TechSupport
NXP TechSupport

Hello @mmt45 

I hope you are doing well.

 

Could you please contact to your sales person?

We cannot provide support for this board.

 

Best regards,

--... ...--

Salas.

0 件の賞賛
返信

2,311件の閲覧回数
mmt45
Contributor I

Screenshot from 2024-08-19 15-10-21.pngScreenshot from 2024-08-19 15-10-21.png

this is another screenshot from the terminal

0 件の賞賛
返信