Fast ethernet controller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Fast ethernet controller

9,789件の閲覧回数
gri
Contributor I
Hello,
I'm searching for a application note for the FEC, it should containt a schematic how to connect the cpu with ethernet connector and some sample code.

Regards
タグ(2)
0 件の賞賛
返信
9 返答(返信)

5,508件の閲覧回数
laurentiu
Contributor I
Hi,
 
Regarding FEC module for MPC5553 I have some problems with DMA and FIFO Controller. After a write to TDAR a frame is transmitted correctly, but after I set up another transmit frame and write to TDAR no frame is transmitted. It seems that DMA and the RISC Controller doesn't read the following buffer descriptors. Do you have a hint for this?
 
Thanks
0 件の賞賛
返信

5,508件の閲覧回数
laurentiu
Contributor I
I fount out the solution to the problem I had few days ago. A detailed explanation of this issue and a workaround for it can be found in Errata 2049 in the attached file.
 
Message Edited by t.dowe on 2009-10-20 01:15 PM
0 件の賞賛
返信

5,508件の閲覧回数
RickN
Contributor I
See attached EVB schematics.
 
Cheers,
 
  Rick
 
Message Edited by t.dowe on 2009-10-20 01:05 PM
0 件の賞賛
返信

5,508件の閲覧回数
gri
Contributor I
Thanks for the schematics. In the datasheet I've seen that the pins for the FEC are only available in the 416 pin BGA. This BGA is a bit to large, I want to use the 324 pin BGA or even the smaller 208 pin BGA. Is it possible to route the FEC pins to other GPIO pins using the crossbar?

Regards

0 件の賞賛
返信

5,508件の閲覧回数
RickN
Contributor I
Hi,
 
  Sorry, but you need to have the package with the FEC pinned out.
 
 
- Rick
0 件の賞賛
返信

5,508件の閲覧回数
gri
Contributor I
The FEC shares pins with the data bus, is it possible to use the fec and the ebi for memory in the same time?
0 件の賞賛
返信

5,508件の閲覧回数
gri
Contributor I
Hello,
where is pin 7 of the DP83848, PWR_DWN, connected. I'm unable to search insinde the pdf.

Regards
0 件の賞賛
返信

5,508件の閲覧回数
gri
Contributor I
For the MPC5553. At the beginning a schematic is engough.

Regards

0 件の賞賛
返信

5,507件の閲覧回数
RickN
Contributor I
Which MPU?
0 件の賞賛
返信