Unable to flash bsp

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to flash bsp

2,324 Views
srisindhu
Contributor I
hi,
    I have imx21ads board and iam trying to install bsp in linux 2.4 version(fedora). I have followed steps given for installing linux bsp for imxads board.
I have installed bsp and when iam trying to flash the bootloader using the following command,
 
<install_path>/bin/imx21_download -- port  /dev/ttyS0  --addr \0xc0300000  --stop_auto_boot <install_path>/rootfs/boot/blob
 
 iam getting following error:-
version glibc_2.4.lib not found.
 
can anyone help in resolving this.
 
 
0 Kudos
Reply
1 Reply

1,704 Views
mr_venkatarao
Contributor I
Hi sindhu..i am not solving your problem but it is better to submit service request to freescale. Then it will be resolved much better in less time..
 
venki....
0 Kudos
Reply