FS6500 hardware sleep

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FS6500 hardware sleep

Jump to solution
2,191 Views
smichael
Contributor II

Hi,

   Is that possible to put the FS6550 in sleep mode using any IO or through hardware?

In datasheet it seems through SPI only possible there is no other way.guoweisun

0 Kudos
Reply
1 Solution
2,131 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

One additional case except use SPI command:

---

Connect SELECT pin to VPRE,then if FS6500 RSTB assert and keep low more than 8s,then FS6500 enter into SLEEP mode.

---

View solution in original post

0 Kudos
Reply
1 Reply
2,132 Views
guoweisun
NXP TechSupport
NXP TechSupport

HI

One additional case except use SPI command:

---

Connect SELECT pin to VPRE,then if FS6500 RSTB assert and keep low more than 8s,then FS6500 enter into SLEEP mode.

---

0 Kudos
Reply