FS6500 hardware sleep

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FS6500 hardware sleep

跳至解决方案
2,177 次查看
smichael
Contributor II

Hi,

   Is that possible to put the FS6550 in sleep mode using any IO or through hardware?

In datasheet it seems through SPI only possible there is no other way.guoweisun

0 项奖励
回复
1 解答
2,117 次查看
guoweisun
NXP TechSupport
NXP TechSupport

HI

One additional case except use SPI command:

---

Connect SELECT pin to VPRE,then if FS6500 RSTB assert and keep low more than 8s,then FS6500 enter into SLEEP mode.

---

在原帖中查看解决方案

0 项奖励
回复
1 回复
2,118 次查看
guoweisun
NXP TechSupport
NXP TechSupport

HI

One additional case except use SPI command:

---

Connect SELECT pin to VPRE,then if FS6500 RSTB assert and keep low more than 8s,then FS6500 enter into SLEEP mode.

---

0 项奖励
回复