Error on MML09212H 's Datasheet

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error on MML09212H 's Datasheet

Jump to solution
1,496 Views
ricardopereira
Contributor I

Hi, in the schematic of MML09212H you say that R1 is connected to pin 12, but on the layout you connect it to pin 10. Which one is correct?

Thank you for your time.

0 Kudos
Reply
1 Solution
1,415 Views
LPP
NXP Employee
NXP Employee

You are right, in the datasheet connection of R1C7 in the schematics differs from that in the layout.
Though, the connection order of R1C7 to pins 10,12 or pins 12,10 does not matter. Both provides the same functionality.

So, we have no serious reasons to fix this discrepancy in the datasheet.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,416 Views
LPP
NXP Employee
NXP Employee

You are right, in the datasheet connection of R1C7 in the schematics differs from that in the layout.
Though, the connection order of R1C7 to pins 10,12 or pins 12,10 does not matter. Both provides the same functionality.

So, we have no serious reasons to fix this discrepancy in the datasheet.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply