Error on MML09212H 's Datasheet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error on MML09212H 's Datasheet

跳至解决方案
1,491 次查看
ricardopereira
Contributor I

Hi, in the schematic of MML09212H you say that R1 is connected to pin 12, but on the layout you connect it to pin 10. Which one is correct?

Thank you for your time.

0 项奖励
回复
1 解答
1,410 次查看
LPP
NXP Employee
NXP Employee

You are right, in the datasheet connection of R1C7 in the schematics differs from that in the layout.
Though, the connection order of R1C7 to pins 10,12 or pins 12,10 does not matter. Both provides the same functionality.

So, we have no serious reasons to fix this discrepancy in the datasheet.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,411 次查看
LPP
NXP Employee
NXP Employee

You are right, in the datasheet connection of R1C7 in the schematics differs from that in the layout.
Though, the connection order of R1C7 to pins 10,12 or pins 12,10 does not matter. Both provides the same functionality.

So, we have no serious reasons to fix this discrepancy in the datasheet.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复