Error on MML09212H 's Datasheet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error on MML09212H 's Datasheet

ソリューションへジャンプ
1,490件の閲覧回数
ricardopereira
Contributor I

Hi, in the schematic of MML09212H you say that R1 is connected to pin 12, but on the layout you connect it to pin 10. Which one is correct?

Thank you for your time.

0 件の賞賛
返信
1 解決策
1,409件の閲覧回数
LPP
NXP Employee
NXP Employee

You are right, in the datasheet connection of R1C7 in the schematics differs from that in the layout.
Though, the connection order of R1C7 to pins 10,12 or pins 12,10 does not matter. Both provides the same functionality.

So, we have no serious reasons to fix this discrepancy in the datasheet.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,410件の閲覧回数
LPP
NXP Employee
NXP Employee

You are right, in the datasheet connection of R1C7 in the schematics differs from that in the layout.
Though, the connection order of R1C7 to pins 10,12 or pins 12,10 does not matter. Both provides the same functionality.

So, we have no serious reasons to fix this discrepancy in the datasheet.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信