Control of outputs of MC33882 output switch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Control of outputs of MC33882 output switch

Jump to solution
1,653 Views
ondrej_brejla
Contributor I

Hi,

I´m planning on using the MC33882 for realisation of digital outputs on a project I´m working on. I'm going to use the SPI interface to control the outputs. It's not really clear to me what should I do with the remaining input pins (IN0...IN7 and IN0&IN1 … IN4&IN5). Is it better to connect them to GND or just leave them with their internal pull down? Also should the unused outputs be left unconnected ?

Best regards,

Ondrej Brejla

0 Kudos
Reply
1 Solution
1,596 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

For IN you can connect them to GND,for outputs you can floating.

Thanks!

View solution in original post

1 Reply
1,597 Views
guoweisun
NXP TechSupport
NXP TechSupport

Hi,

For IN you can connect them to GND,for outputs you can floating.

Thanks!