Hi,
I´m planning on using the MC33882 for realisation of digital outputs on a project I´m working on. I'm going to use the SPI interface to control the outputs. It's not really clear to me what should I do with the remaining input pins (IN0...IN7 and IN0&IN1 … IN4&IN5). Is it better to connect them to GND or just leave them with their internal pull down? Also should the unused outputs be left unconnected ?
Best regards,
Ondrej Brejla
Solved! Go to Solution.
Hi,
For IN you can connect them to GND,for outputs you can floating.
Thanks!
Hi,
For IN you can connect them to GND,for outputs you can floating.
Thanks!