Codewarrior Tap connection issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Codewarrior Tap connection issues

ソリューションへジャンプ
2,548件の閲覧回数
Ghouse
Contributor V

Hi, iam using LS1046ARDB eval board,

i also have Codewarrior USB TAP, and i have installed Codewarrior Software in the Linux machine,

Now when i have opened Codewarrior and trying to debug the Eval board, it sometimes connects and sometimes it doesn't, it throws the following error in connection diagnostics "failed to connect to locally started codewarrior connection server"

I also have a floating license for codewarrior, and when i have connected the codewarrior usb tap, iam unable to connect to the network and hence unable to fetch the floating license from the server.

Please guide me in sorting above issues

Thanks.

タグ(1)
0 件の賞賛
返信
1 解決策
2,510件の閲覧回数
Ghouse
Contributor V

hi, thank you for the reply, that helped in resolving the issue, request to kindly add those instructions/commands in the code warrior tap manual

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,521件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please open CodeWarrior IDE and check the license from Help->NXP Licenses.

Please invoke CCS console. 

$ sudo Freescale/CW4NET_v2020.06/Common/CCS/bin/ccs

and type the following command to do verification.

% config cc cwtap

% show cc

% source IDcode.tcl

0 件の賞賛
返信
2,511件の閲覧回数
Ghouse
Contributor V

hi, thank you for the reply, that helped in resolving the issue, request to kindly add those instructions/commands in the code warrior tap manual

0 件の賞賛
返信