Codewarrior Tap connection issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Codewarrior Tap connection issues

Jump to solution
2,554 Views
Ghouse
Contributor V

Hi, iam using LS1046ARDB eval board,

i also have Codewarrior USB TAP, and i have installed Codewarrior Software in the Linux machine,

Now when i have opened Codewarrior and trying to debug the Eval board, it sometimes connects and sometimes it doesn't, it throws the following error in connection diagnostics "failed to connect to locally started codewarrior connection server"

I also have a floating license for codewarrior, and when i have connected the codewarrior usb tap, iam unable to connect to the network and hence unable to fetch the floating license from the server.

Please guide me in sorting above issues

Thanks.

Tags (1)
0 Kudos
Reply
1 Solution
2,516 Views
Ghouse
Contributor V

hi, thank you for the reply, that helped in resolving the issue, request to kindly add those instructions/commands in the code warrior tap manual

View solution in original post

0 Kudos
Reply
2 Replies
2,527 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please open CodeWarrior IDE and check the license from Help->NXP Licenses.

Please invoke CCS console. 

$ sudo Freescale/CW4NET_v2020.06/Common/CCS/bin/ccs

and type the following command to do verification.

% config cc cwtap

% show cc

% source IDcode.tcl

0 Kudos
Reply
2,517 Views
Ghouse
Contributor V

hi, thank you for the reply, that helped in resolving the issue, request to kindly add those instructions/commands in the code warrior tap manual

0 Kudos
Reply