CodeWarrior USB Tap connector pitch

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior USB Tap connector pitch

Jump to solution
1,480 Views
WO1
Contributor II

Hi.

I am designing a PCB and I want to include a 14-pin header to connect directly to CodeWarrior USB Tap. I can't seem to find any information regarding the connector pitch. Any help is appreciated.

Thanks

0 Kudos
Reply
1 Solution
1,470 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the 14 pin JTAG pin connector on the PCB which can interface with USBTAP device or multilink universal, the connector is a standard connector, the pitch is 100mil or 2.54mm.

pls select the right male 14 pin connector with 100 mil pitch.

Hope it can help you

BR

XiangJun Rong

 

View solution in original post

0 Kudos
Reply
1 Reply
1,471 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the 14 pin JTAG pin connector on the PCB which can interface with USBTAP device or multilink universal, the connector is a standard connector, the pitch is 100mil or 2.54mm.

pls select the right male 14 pin connector with 100 mil pitch.

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply