CodeWarrior USB Tap connector pitch

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CodeWarrior USB Tap connector pitch

ソリューションへジャンプ
1,481件の閲覧回数
WO1
Contributor II

Hi.

I am designing a PCB and I want to include a 14-pin header to connect directly to CodeWarrior USB Tap. I can't seem to find any information regarding the connector pitch. Any help is appreciated.

Thanks

0 件の賞賛
返信
1 解決策
1,471件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the 14 pin JTAG pin connector on the PCB which can interface with USBTAP device or multilink universal, the connector is a standard connector, the pitch is 100mil or 2.54mm.

pls select the right male 14 pin connector with 100 mil pitch.

Hope it can help you

BR

XiangJun Rong

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,472件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

For the 14 pin JTAG pin connector on the PCB which can interface with USBTAP device or multilink universal, the connector is a standard connector, the pitch is 100mil or 2.54mm.

pls select the right male 14 pin connector with 100 mil pitch.

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信