Can i put TEF82XX RfeCalibration in the child thread?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can i put TEF82XX RfeCalibration in the child thread?

ソリューションへジャンプ
1,028件の閲覧回数
Shi_test
Contributor III

S32R45: There is a lot of time with Calibration,so i want to put the RF Calibration in child thread.Is there anything I should notice?

Shi_test_0-1700441108738.png

 

0 件の賞賛
返信
1 解決策
1,002件の閲覧回数
GaryRK
NXP Employee
NXP Employee

Hi Shi_test,

Yes you could execute the RsdkRfeCalibration() function in a different thread but you need to make sure the calibration operation completes before triggering the start of radar frame.

Best regards,

Gary

元の投稿で解決策を見る

2 返答(返信)
1,003件の閲覧回数
GaryRK
NXP Employee
NXP Employee

Hi Shi_test,

Yes you could execute the RsdkRfeCalibration() function in a different thread but you need to make sure the calibration operation completes before triggering the start of radar frame.

Best regards,

Gary

1,013件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

In order to get accurate answer from RADAR SW team can you please submit a ticket at NXP.com so I can escalate this to RADAR team?

https://community.nxp.com/t5/HomeTest-Knowledge-Base/How-to-submit-a-new-question-for-NXP-Support/ta...

I will ask some colleagues from RADAR team for quick feedback ASAP. and post it here also.

Best regards,

Peter