Can i put TEF82XX RfeCalibration in the child thread?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Can i put TEF82XX RfeCalibration in the child thread?

跳至解决方案
1,029 次查看
Shi_test
Contributor III

S32R45: There is a lot of time with Calibration,so i want to put the RF Calibration in child thread.Is there anything I should notice?

Shi_test_0-1700441108738.png

 

0 项奖励
回复
1 解答
1,003 次查看
GaryRK
NXP Employee
NXP Employee

Hi Shi_test,

Yes you could execute the RsdkRfeCalibration() function in a different thread but you need to make sure the calibration operation completes before triggering the start of radar frame.

Best regards,

Gary

在原帖中查看解决方案

2 回复数
1,004 次查看
GaryRK
NXP Employee
NXP Employee

Hi Shi_test,

Yes you could execute the RsdkRfeCalibration() function in a different thread but you need to make sure the calibration operation completes before triggering the start of radar frame.

Best regards,

Gary

1,014 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

In order to get accurate answer from RADAR SW team can you please submit a ticket at NXP.com so I can escalate this to RADAR team?

https://community.nxp.com/t5/HomeTest-Knowledge-Base/How-to-submit-a-new-question-for-NXP-Support/ta...

I will ask some colleagues from RADAR team for quick feedback ASAP. and post it here also.

Best regards,

Peter