CDMA decode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CDMA decode

Jump to solution
2,603 Views
jessesun
Contributor I

Hi,

I using TEF82XX enables CDMA(MIMO) signal. If the s32r45 can be using to decode the MIMO signal? Is there any sample I can reference?

#TEF82XX

#S32R45

Tags (2)
0 Kudos
Reply
1 Solution
2,541 Views
petervlna
NXP TechSupport
NXP TechSupport
0 Kudos
Reply
3 Replies
2,578 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes it can be used for such purpose. However all available example codes are in RTD package

petervlna_1-1692950137969.png

But I am not sure whether there is processing of TEF82xx signals implemented in some libraries or so as we do not have demo board for TEF82xx and S32R45. Most probably there is no such solution available.

Best regards,

Peter

 

 

0 Kudos
Reply
2,572 Views
jessesun
Contributor I

Hi Peter,

Thank you for your reply. Another question is that where I can get example codes are in RTD package of s32r45 as I check that I have no these codes. 

Best Regrads,

Jesse

 

0 Kudos
Reply
2,542 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

You can get it from our web page of S32R45:

https://www.nxp.com/products/processors-and-microcontrollers/s32-automotive-platform/s32r-radar-proc...

petervlna_0-1693205319197.png

Best regards,

Peter

0 Kudos
Reply