CD1020 debouncing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CD1020 debouncing

Jump to solution
910 Views
Andam3141
Contributor I

On device datasheet is reported the value of "input glitch timer filter"  between 5us and 18us without any additional data.

Andam3141_0-1748359071203.png

Does this parameter refer to a debounce timer?

This debounce timer is active on all input channels (SG/SB)?

This debounce timer is programmable or the range is due to tolerance?

Thanks,

Regards,

Andrea

 

Tags (1)
0 Kudos
Reply
1 Solution
886 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello!

Does this parameter refer to a debounce timer? yes

This debounce timer is active on all input channels (SG/SB)? yes

This debounce timer is programmable or the range is due to tolerance? it is not programmable. this is due to tolerance.

View solution in original post

0 Kudos
Reply
1 Reply
887 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello!

Does this parameter refer to a debounce timer? yes

This debounce timer is active on all input channels (SG/SB)? yes

This debounce timer is programmable or the range is due to tolerance? it is not programmable. this is due to tolerance.

0 Kudos
Reply