CD1020 debouncing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
913件の閲覧回数
Andam3141
Contributor I

On device datasheet is reported the value of "input glitch timer filter"  between 5us and 18us without any additional data.

Andam3141_0-1748359071203.png

Does this parameter refer to a debounce timer?

This debounce timer is active on all input channels (SG/SB)?

This debounce timer is programmable or the range is due to tolerance?

Thanks,

Regards,

Andrea

 

タグ(1)
0 件の賞賛
返信
1 解決策
889件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello!

Does this parameter refer to a debounce timer? yes

This debounce timer is active on all input channels (SG/SB)? yes

This debounce timer is programmable or the range is due to tolerance? it is not programmable. this is due to tolerance.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
890件の閲覧回数
ErikaC
NXP TechSupport
NXP TechSupport

Hello!

Does this parameter refer to a debounce timer? yes

This debounce timer is active on all input channels (SG/SB)? yes

This debounce timer is programmable or the range is due to tolerance? it is not programmable. this is due to tolerance.

0 件の賞賛
返信