56800E application loader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

56800E application loader

2,550件の閲覧回数
admin
Specialist II
I use CWv8 & PE to create loader for 56F8323 mcu. I want to load my application in to boot flash. if i use default settings compiled project ready to load in to the program flash. What can i do put code in to the boot?
0 件の賞賛
返信
1 返信

1,618件の閲覧回数
admin
Specialist II
OK.

I have found only one method - change linker (.cmd) file - put execute code in to the boot flash. But I think when Processor Expert is used this is not very flexible way - need to disable linker file generation, manually edit linker file. Or I missed something?

What are you think about it?
0 件の賞賛
返信