56800E application loader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

56800E application loader

2,551 Views
admin
Specialist II
I use CWv8 & PE to create loader for 56F8323 mcu. I want to load my application in to boot flash. if i use default settings compiled project ready to load in to the program flash. What can i do put code in to the boot?
0 Kudos
Reply
1 Reply

1,619 Views
admin
Specialist II
OK.

I have found only one method - change linker (.cmd) file - put execute code in to the boot flash. But I think when Processor Expert is used this is not very flexible way - need to disable linker file generation, manually edit linker file. Or I missed something?

What are you think about it?
0 Kudos
Reply