380--450 MHz UHF BROADBAND DXF-Gerber layout

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

380--450 MHz UHF BROADBAND DXF-Gerber layout

ソリューションへジャンプ
2,159件の閲覧回数
franco_bocalon
Contributor I

Hi, exist the layout for the  380--450 MHz UHF Broadband, 136--174 MHz VHF Broadband, or the 450--520 MHz UHF broadband?

Into the product page only is provided a dxf file for the  520 MHz Narrowband application. 

Below is the layout file that I am looking for:
 

pastedImage_1.png

Best Regards

Franco

タグ(3)
0 件の賞賛
返信
1 解決策
2,058件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Provided by direct email.

元の投稿で解決策を見る

3 返答(返信)
2,058件の閲覧回数
franco_bocalon
Contributor I

Dear Andrei,

Great! Thank you. How about the other networks for the 136--174 MHz VHF Broadband and the 450--520 MHz UHF broadband?
The board have small changes but if you could provide the dxf board that would be great.


Best Regards

Franco

0 件の賞賛
返信
2,059件の閲覧回数
andrei_skok
NXP Employee
NXP Employee

Provided by direct email.

1,516件の閲覧回数
nicks135
Contributor I

can you share dxf files for 136--174 MHz VHF Broadband and the 380--450 MHz UHF broadband with me too? if possible plzz share gerber as well.

 

0 件の賞賛
返信