380--450 MHz UHF BROADBAND DXF-Gerber layout

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

380--450 MHz UHF BROADBAND DXF-Gerber layout

跳至解决方案
2,158 次查看
franco_bocalon
Contributor I

Hi, exist the layout for the  380--450 MHz UHF Broadband, 136--174 MHz VHF Broadband, or the 450--520 MHz UHF broadband?

Into the product page only is provided a dxf file for the  520 MHz Narrowband application. 

Below is the layout file that I am looking for:
 

pastedImage_1.png

Best Regards

Franco

标记 (3)
0 项奖励
回复
1 解答
2,057 次查看
andrei_skok
NXP Employee
NXP Employee

Provided by direct email.

在原帖中查看解决方案

3 回复数
2,057 次查看
franco_bocalon
Contributor I

Dear Andrei,

Great! Thank you. How about the other networks for the 136--174 MHz VHF Broadband and the 450--520 MHz UHF broadband?
The board have small changes but if you could provide the dxf board that would be great.


Best Regards

Franco

0 项奖励
回复
2,058 次查看
andrei_skok
NXP Employee
NXP Employee

Provided by direct email.

1,515 次查看
nicks135
Contributor I

can you share dxf files for 136--174 MHz VHF Broadband and the 380--450 MHz UHF broadband with me too? if possible plzz share gerber as well.

 

0 项奖励
回复