Problems with USBDM installation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problems with USBDM installation

9,412 Views
adrik456
Contributor I

Hi all, I'm trying to install USBDM for use with a JS16 adapter (Ebay). If I install the USBDM V4.12 with the default settings it crashes badly during installation. So i have removed all unwanted features leaving only what i need (HCS08 & RS08 programmers). In this manner the installation work, but the programmers dont. No errors are shown, but, when i try to launch a programmer, the result is only a little flashing of the hd led. The task manager confirm that a process named HCS08_Flashprogrammer is started but a few seconds later the process is terminated. Same result with older releases of USBDM downloaded from sourceforge, and on three other PC all running WXP Professional.

The hardware seems to work properly, i can reprogram the chip and verify the result with no errors.

What i'm doing wrong?? any clues??

Thanks.

Tags (1)
0 Kudos
Reply
18 Replies

8,702 Views
pgo
Senior Contributor V

Hi Adriano,

I have installed Win-XP 32-bit in a virtual machine on a Windows 8 machine.

pastedImage_1.png

I had trouble installing the drivers and have found the reason for that but I had no problems in installing or running the applications (except for being very slow). 

I have been unable to locate a WINXP-64bit VM image.  What version are you running *32/64-bit?

There might also be a problem with language version of windows but I have no real experience with this.

bye

0 Kudos
Reply

8,702 Views
adrik456
Contributor I

Hi pgo,

Attached the image of MergeXML. It says that 2 DLL's are missing. A message on

MS forum says that those DLL's are used on Vista and successive release.

I've tried to download the DLL's but there are so many variants, and i dont know

what is the correct one.

I'm using WXP 32bit on Intel & AMD x86.

Many thanks,

Adriano

0 Kudos
Reply

8,702 Views
pgo
Senior Contributor V

Hi Adriano,

I don't believe the problem is due to the DLLs you have mentioned.  These are delay-loaded by DLLs within windows and not actually used by the USBDM DLLs.

It would appear that all the DLLs provided by USBDM are finding all their entry points in the supplied DLLs so that looks an unhelpful path.

Could you try the following:

  • Open a command window
  • Change directory to C:\Program Files (x86)\pgo\USBDM 4.12.1.150 
  • Run UsbdmFlashProgrammer-debug.exe and see if it reports any errors when launched.
  • Check for a log file Flashprogrammer.log in %APPDATA%\usbdm  and post it if it exists.

bye

0 Kudos
Reply

8,702 Views
adrik456
Contributor I

Hi pgo,

Attached the files generated after a crash.

Thank you, ciao.

Adriano

0 Kudos
Reply

8,702 Views
pgo
Senior Contributor V

Hi Adriano,

The log files seem to confirm that the problem lies in Xerces-C DLL.  I haven't had any luck coming up with ideas of why this would be occurring.

Could you try using the memory dump program which doesn't use Xerces to see if it operates correctly?

I have uploaded a new test version of USBDM to Sourceforge which uses (amongst other things) a different version of the Xerces DLL.  This may have some impact on the problem.  Could you try this please?

bye

0 Kudos
Reply

8,702 Views
adrik456
Contributor I

Hi pgo,

I was thinking that one of the PC on which I tried to install USBDM had WXPSp3

in USA language, on which I could install several language packs. So I think

that even the installation language is the wrong way. Can you send me the length

of the various files obtained after installation, to check that they are

properly recovered?

Did you get my last message related to WIN-7 sp1 on 02/15/2017 ?

Thanks, ciao.

Adriano

0 Kudos
Reply

8,702 Views
pgo
Senior Contributor V

Hi Adriano,

I can't find a posting with that date and I haven't received a PM, so I'm unsure which message you are referring to.

I am uploading a zip of the installation image for 4_12.1.150 to sourceforge which you can use to check sizes.  I will delete it in a few days.

It is very unlikely the installer is changing files.

bye

0 Kudos
Reply

8,702 Views
adrik456
Contributor I

Hi pgo,

I can not find the zip file on SourceForge.

Could you send me a link to this file?

Thanks, Ciao,

Adriano

0 Kudos
Reply

8,702 Views
adrik456
Contributor I

Hi pgo,

since it seems that you have not received my message (lost in space??) I am

attaching again.

The original msg was sent on 01/16/2017 00:32 GMT+1.

--> Sorry to have to inform you that the new release of USBDM not work either

under WXPsp3 nor under W7sp1.

The culprit is as always "mergexml". Since I have tried six PCs with different

operating systems and with Intel and AMD CPU and all have the same problem there

has to be a common cause: perhaps the language of my OS?

"Memory Dump", "Firmware Updater" & "JS1 ..." works properly. I enclose the

crash report generated from Win7 and WXP. <--

Thanks, ciao.

Adriano

0 Kudos
Reply

8,702 Views
pgo
Senior Contributor V

Hi Adriano,

I left it uploading last night but it appears to have failed - possible because it was too big.

I have attached recursive directory listing which are probably more sensible.

bye

0 Kudos
Reply

8,701 Views
adrik456
Contributor I

Hi pgo,

Attached the USBDM installation structure on my PC.

While the length of the files matches yours, some folders are missing.

I think they are necessary only during compilation of the project, but it is not

that I miss some important files?

Thanks, ciao.

Adriano

0 Kudos
Reply

8,701 Views
pgo
Senior Contributor V

Hi Adriano,

I provided 3 listings.  Two were for the build directories and one for an actual installation.  The build directories have extra folders as you have indicated.

I'm sorry but I can't see how I can make any progress on this.  The problem may well be a  language related error but since it is occurring in the Xerces DLL I can't see any way of debugging it since I can't repeat the error.

What language is your Windows installations?  It is unlikely that I will be able to find a version to install but I can have a look.

bye

0 Kudos
Reply

8,701 Views
adrik456
Contributor I

Hi pgo,

As you can see on the attached file, in my installation the "Stationery" folder

is missing. I dont know if it is needed. My installation is in Italian language.

Ciao,

Adriano

0 Kudos
Reply

8,696 Views
pgo
Senior Contributor V

Hi Adriano,

The Stationery folder is part of the eclipse plugin and would not be created if that option was not installed.

One thing to try (to check another point) is to rename the DeviceData directory and see if the programmer still crashes.

bye

0 Kudos
Reply

8,701 Views
adrik456
Contributor I

Hi pgo,

If I rename the "DeviceData" dir, then run the "HCS08 Programmer" the "USBDM

installer" starts, reinstalls a fresh copy of "DeviceData" and then it crashes

with the usually message :smileysad: (Applicazione che ha provocato l'errore

usbdmflashprogrammer.exe, versione 4.12.1.160, modulo che ha provocato l'errore

libxerces-c-3-1.dll, versione 0.0.0.0, indirizzo errore 0x000072f8)

Ciao,

Adriano

0 Kudos
Reply

8,700 Views
pgo
Senior Contributor V

Hi Adriano,

Unfortunately I no longer have access to WINXP machines for testing so the USBDM installer is no longer tested on that platform.

I am not aware of any changes that would prevent installation but that means little I'm afraid.

You can try running the installer with options for creating a log file which might indicate the problem. You may need to edit the attached file so that is references the correct installer name.

Please post the copious log file.

Can you be specific about which installation option is failing?

In the mean time I'll see which features are missing when Programmers are installed by themselves.

bye

PS. It is unlikely that a eBay programmer will support RS08 devices.  RS08 required a switched 12V supply which is a rarity in the commercial programmers.

=============

Follow Up

I have tested installing with only the Programmer option selected.  It appears to install correctly and function correctly, so it seems likely that there is some incompatibility with WINXP in general that is causing a problem rather than specifically an installer problem.  It is possible that there is a problem with MinGW libraries or similar.  Do you have MinGW installed?

bye

0 Kudos
Reply

8,700 Views
adrik456
Contributor I

Hi pgo,

Thank you for your kind reply.

To isolate the problem i've dedicated the fifth pc to USBDM.

This is a very old Acer 525TX laptop (PIII 800MHz, 512MB ram) with a "fresh &

clean" WXPsp3 OS installation. The only app. installed is Firefox. The other

PC's (4) on wich i've installed USBDM have al least CW6.3 plus oher non NXP mcu

packages.

The USBDM installation (4.12.1.150b), leaving only the programmers installed and

NO drivers installed, come flawlessy to the end without any error (NO CW6.3

installed so the installer disables the connection by default).

When i've tried to launch the HCS08 programmer the program crashes. Please see

USBDM#1 screenshot on attached file. The culprit seems to be the

"libxerces-c-3-1.dll" (USBDM#2, USBDM#3); this error appears on all my

installation. Then i've installed the drivers (USBDM_Drivers_4_12_1_WinXP_x32).

The installation failed with the message in USBDM#4.

I've found on NXP community a message (USBDM programmers problem; Dorin Horvath

il 6-gen-2014; https://community.nxp.com/thread/317629 ) that reports the same

problem i'm having.

In my system, two XML files are generated (HCS08_Testdevices &

HCS08_unsupported) that, while can be opened by a text editor, cannot be opened

by firefox or IE. Both reports an error in XML file.

Then i have installed 1.3.0 drivers. They have a strange behaviour: only the

com port e USBDM driver is installed (no JS16), and removing the harware from

USB and reconnecting it, the com port cannot be seen again in device manager.

With a new installation of 1.1.0 drivers, all things are installed ok (USBDM,

COM Port, JS16) but the programmer still not work.

The install log file attached has been obtained on another PC with CW6.3

installed, so the relative option is enabled by default.

The crash is reported in USBDM#5.

Hope it can help you to find a solution.

Do you have a release fully tested on XP machine?

Where can i find it?

Thank you so much,

Adriano

il 12/02/2017 pgo ha scritto:

0 Kudos
Reply

8,700 Views
pgo
Senior Contributor V

Hi Adriano,

I suspect the problem is an incompatibility with MinGW libraries.  There are some problems with different versions of the windows DLLs.

It is unlikely to be a problem with the XML files since they are unchanged on different OSs.  The files you mention are not valid XML as they are only fragments that are used in other files.

Could you try dependency walker on the Xerces dll and see if indicates missing dependencies?

I will try to locate a Win-XP installation disk and see if I can run it in a virtual machine to see if there are similar errors.

bye

0 Kudos
Reply