CLI BDM Programmer for ColdFire V2 on Linux or Windows

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CLI BDM Programmer for ColdFire V2 on Linux or Windows

5,234 次查看
lucaskt
Contributor I

Hello,

 

I was wondering if there are any CLI (Command Line Interface) USB BDM Flash Programmers for ColdFire V2 for either Linux (preferably) or Windows.

 

I've been trying to perform this recording on Linux via BDM tools (http://sourceforge.net/projects/bdm/) , and so far have been unsucessful.

 

I was also wondering if the default Code Warrior recorder can be used outside the IDE, or is it built-in?

 

Thanks for any replies.

Lucas

标记 (2)
0 项奖励
回复
2 回复数

1,477 次查看
greg_b
Contributor I
0 项奖励
回复

1,477 次查看
diep
Contributor I

Hi

If I use "CLI BDM Programmer for ColdFire V2 on Linux or Windows", what hardware tool do I have to use to programming for MCF5271?

thank

0 项奖励
回复